Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE, TIDM-DC-DC-BUCK, C2000WARE-DIGITALPOWER-SDK
Tool/software:
HI all,
I am trying to implement state machine based tasks in 28027. I referred some programmes given in control suite. I am however not able to go between various tasks A0, A1, A2 etc. What could be the reason for this.
I am attaching the code for your reference. It also goes to ESTOP 0 after few seconds.
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
#include "MATH_EMAVG_IQ.h"
#include "Solar_IQ.h"
#include "IQmathLib.h"
#include <math.h>
#include "VARIABLES_CONSTANTS.h"
// -------------------------------- FRAMEWORK --------------------------------------
// State Machine function prototypes
//----------------------------------------------------------------------------------
// Alpha states
void A0(void); //state A0
// A branch states
void A1(void); //state A1
void A2(void); //state A2
void A3(void); //state A3
void A4(void); //state A4
int A0_State=0, A1_State=0, A2_State=0, A3_State=0, A4_State=0;
// Variable declarations
void (*Alpha_State_Ptr)(void); // Base States pointer
void (*A_Task_Ptr)(void); // State pointer A branch
//%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
// VARIABLE DECLARATIONS - GENERAL
//%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
// -------------------------------- FRAMEWORK --------------------------------------
int16 VTimer0[4]; // Virtual Timers slaved off CPU Timer 0
int16 VTimer1[4]; // Virtual Timers slaved off CPU Timer 1
int16 VTimer2[4]; // Virtual Timers slaved off CPU Timer 2
void main(void)
{
InitSysCtrl();
MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart);
InitFlash();
// Step 4. Initialize the Device Peripheral. This function can be
// found in DSP2802x_CpuTimers.c
InitCpuTimers(); // For this example, only initialize the Cpu Timers
// Timing sync for background loops
// Timer period definitions found in PeripheralHeaderIncludes.h
//ConfigCpuTimer(struct CPUTIMER_VARS *Timer, float Freq, float Period)
//CpuTimer0Regs.PRD.all = 60000 ; // A tasks
ConfigCpuTimer(&CpuTimer0, 60, 1000000);
// Tasks State-machine init
Alpha_State_Ptr = &A0;
A_Task_Ptr = &A1;
VTimer0[0] = 0;
DINT;
InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
EDIS;
CpuTimer0Regs.TCR.all = 0x4001; // Use write-only instruction to set TSS bit = 0
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
EDIS;
// Enable CPU int1 which is connected to CPU-Timer 0, CPU int13
// which is connected to CPU-Timer 1, and CPU int 14, which is connected
// to CPU-Timer 2:
IER |= M_INT1;
IER |= M_INT3;
// Enable EPWM INTn in the PIE: Group 3 interrupt 1-3
// PieCtrlRegs.PIEIER1.bit.INTx1 = 1; // Enable INT 1.1 in the PIE
PieCtrlRegs.PIEIER3.bit.INTx2 = 1;
PieCtrlRegs.PIEIER1.bit.INTx7 = 1; // Enable INT 1.7 (Timer 0 interrupt)
CpuTimer0Regs.TCR.bit.TIE = 1;
// Enable global Interrupts and higher priority real-time debug events:
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
//--------------------------------- FRAMEWORK -------------------------------------
for(;;) //infinite loop
{
// State machine entry & exit point
//===========================================================
(*Alpha_State_Ptr)(); // jump to an Alpha state (A0,B0,...)
//===========================================================
}
} //END MAIN CODE
//=================================================================================
// STATE-MACHINE SEQUENCING AND SYNCRONIZATION
//=================================================================================
//--------------------------------- FRAMEWORK -------------------------------------
void A0(void)
{
// loop rate synchronizer for A-tasks
if(CpuTimer0Regs.TCR.bit.TIF == 1)
{
A0_State++;
CpuTimer0Regs.TCR.bit.TIF = 0; // clear flag
//-----------------------------------------------------------
(*A_Task_Ptr)(); // jump to an A Task (A1,A2,A3,...)
//-----------------------------------------------------------
VTimer0[0]++; // virtual timer 0, instance 0 (spare)
}
// Alpha_State_Ptr = &B0; // Comment out to allow only A tasks
}
//=================================================================================
// A - TASKS
//=================================================================================
//--------------------------------------------------------
void A1(void)
//--------------------------------------------------------
{
A1_State++;
// FlagA1++;
//-------------------
//the next time CpuTimer0 'counter' reaches Period value go to A2
A_Task_Ptr = &A2;
//-------------------
}
//-----------------------------------------------------------------
void A2(void)
//-----------------------------------------------------------------
{
A2_State++;
// FlagA2=1;
//-------------------
//the next time CpuTimer0 'counter' reaches Period value go to A1
A_Task_Ptr = &A3;
//-------------------
}
//-----------------------------------------
void A3(void)
//-----------------------------------------
{
A3_State++;
//-----------------
//the next time CpuTimer0 'counter' reaches Period value go to A1
A_Task_Ptr = &A4;
//-----------------
}
//----------------------------------------------------------
void A4(void)
//---------------------------------------------------------
{
A4_State++;
//-----------------
//the next time CpuTimer0 'counter' reaches Period value go to A1
A_Task_Ptr = &A1;
//-----------------
}