Part Number: TMS320F28069
Other Parts Discussed in Thread: DRV8305
Tool/software:
When I did Motor Identification,
the USER_MOTOR_Ls_d and USER_MOTOR_Ls_q values are different depending on the USER_VOLTAGE_FILTER_POLE_Hz value.
Why is that?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28069
Other Parts Discussed in Thread: DRV8305
Tool/software:
When I did Motor Identification,
the USER_MOTOR_Ls_d and USER_MOTOR_Ls_q values are different depending on the USER_VOLTAGE_FILTER_POLE_Hz value.
Why is that?
USER_VOLTAGE_FILTER_POLE_Hz should be calculated correctly according to the voltage filter. You can't set it to the other values you want. The motor control and identify with FAST are related to this parameters.
If I identifycation USER_VOLTAGE_FILTER_POLE_Hz as 583.56(1/(2pi*(30k*3k)/(30k+3k)*0.1*10^-6), the Ld, Lq values are 8*10^-12.
But, this is wrong. If i identification it as 344.618Hz by referring to the DRV8305 design example, i can get the normal value (8*10^-5).
I don't know why.
As mentioned above. The USER_VOLTAGE_FILTER_POLE_Hz is used for estimator. The motor control and identify with FAST are related to this parameters.