Part Number: TMS320F280033
Tool/software:
Hi,
I am going through the 'Technical Reference Manual' for the TMS320F28003x microcontroller. I found that in the Analog subsystem chapter the Pin 'A8' is associated with both 'AIO240' and 'AIO241'. Additionally, this pin is linked to 'CMP4' when both HPMXSEL and LPMXSEL are set to 4.
Could you please clarify which of the two, 'AIO240' or 'AIO241', is connected to the CMP module when the customer selects 'CMP4' with HPMXSEL=4 or LPMXSEL=4?
Thanks
Vinay Khadda