This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28035: TMS320F28035 flag interrupt

Part Number: TMS320F28035

Tool/software:

Hy.

Can you explain how to deal with this?

I have to detect an input interrut at one pin, say XINT1.

Interrupt happens and the servicing routine is executing.

I disable, as first instruction  of isr routine, this interrupt.

If during isr program  executing, another external signal event  generates another flag for this interrupt, when finished isr routine, isr will be called again?

In fact, its flag should remain pending. I want to avoid this; XINT1 interrupt must be enabled when I want and once.

I try to answer to myself: if as first instruction of isr I disable interrupt, no flag can be set.

Enzo