This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P650DK: Program load/flash error in cpu1 on fresh device

Part Number: TMS320F28P650DK


Tool/software:

Hello guyes,

We will going to use TMS320F28650DK6 for our product. We have facing the issue to flash the program in device using CCS. We are getting the error as per mentioned below.

C28xx_CPU1: Error occurred during flash operation: Timed out waiting for target to halt while executing wr_pll.alg
C28xx_CPU1: Error writing the PLL values (Flash algorithm timed out). Operation cancelled.
C28xx_CPU1: Perform a debugger reset and execute the Boot-ROM code (click on the RESUME button in CCS debug window) before erasing/loading the Flash. If that does not help to perform a successful Flash erase/load, check the Reset cause (RESC) register, NMI shadow flag (NMISHDFLG) register and the Boot-ROM status register for further debug.
C28xx_CPU1: File Loader: Memory write failed: Unknown error
C28xx_CPU1: GEL: File: Z:\DevFirm\STC_Master\FNB_STC_Master_FW33.85.xx_2024-12-13\STC_MASTER_3385_CPU1\CPU1_FLASH_STANDALONE\STC_MASTER_3385_CPU1.out: Load failed.

We are using XDS110 to flash the program. Both CPUs are connected successfully, but flashing of devices does not start. Is there need any extra configuration. Please Help us.