Tool/software:
Hi Experts,
I am asking for my customer.
When using MCAN, when there is an error frame on the CAN bus, MCAN will no longer receive and send data, and no related interrupt logic is configured. It can be recovered in a short time, but it cannot be recovered if the error frame lasts too long. However, there is no such problem when using traditional cana. cana has the function of configuring autobusontime, as shown below:

Does mcan also have the same automatic recovery function, or which registers should be configured? Thanks.