Part Number: TMS320F28035
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hello,
I am using TI 28035 experiment kit. I changed my program to run from Flash instead of RAM. It worked once but when I power cycled it stopped working
Referred SPRA958L and its example program but couldn't fix my issue. I am able to run example program "F28035_example_nonBIOS_flash"
Steps followed:
- Replaced 28035_RAM_lnk.cmd with F28035.cmd
- I already had DSP2803x_CodeStartBranch.asm and DSP2803x_Headers_nonBIOS.cmd
- Declared below variables
// Exeternal defines d by the linker
extern Uint16 RamfuncsLoadStart;
extern Uint16 RamfuncsLoadSize;
extern Uint16 RamfuncsRunStart;
- Added below code after function InitPieVectTable();
// Copy Flash-resident functions to RAM
memcpy((Uint16*)&RamfuncsRunStart,(Uint16 *)&RamfuncsLoadStart,
(unsigned long)&RamfuncsLoadSize);
// Enable Flash wait states
InitFlash();
- In function InitPieCtrl, added this code
asm(" EALLOW"); // Enable EALLOW protected register access
// Step around the first three 32-bit locations (six 16-bit locations).
// These locations are used by the ROM bootloader during debug.
memcpy((Uint16 *)&PieVectTable+6, (Uint16 *)&PieVectTableInit+6, 256-6);
asm(" EDIS"); // Disable EALLOW protected register access
Do I have to configure GPIO 37 and GPIO 34 for boot mode?