Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE
Tool/software:
I'm having trouble completing some of the labs on the C2K academy page, namely:
Setting up the ADC in Sysconfig gives me this error in the Pinmux menu. All options default to "Any" which gives an error. However, when I switch to specific GPIO names, it tells me that they're not pinned out on the F28P65x. The program does not work when I try to run it. I'm using C2000Ware 5.03, is this the right SDK for this project and device?

Similarly, when setting up an EQEP in Sysconfig, I also get errors in the Pinmux category. The lab description claims that there should be an option labeled "J12" for EQEP_A, B, and I, however no such option comes up. The program runs fine but the EQEP doesn't seem to be picking up any signals.

I would greatly appreciate if I could get some help with clearing up this confusion. Resources I've found on the launchpad don't seem to give a clear answer as to why the device and the Sysconfig tool seem to be at a mismatch.