Part Number: TMS320F28P559SJ-Q1
Tool/software:
Hi Champ,
Testing F28P559SJ-Q1 in 100-pin package, in debug mode, the GPIO initialized GPAPUD value should be all 1s by default (disabling the pull-up configuration).
It could see few pins' GPAPUD initialized status are set to 0 (Enables the Pull-Up) w/o any code configuration as below screenshot shown in the debug mode - View - Registers window.
However, measuring the pin status in standalone mode, the pins are working properly w/o pull-up to HIGH.
Looking into f28p55.gel, the GPAPUD is assigned with FBFFBFF7 which matches the Debug Registers window.
There should errors in f28p55x GEL file here, could the sw team reconfirm on this ?
(debug mode - View - Registers window)
(f28p55x GEL file)
Thanks and regards,
Johnny