Part Number: TMS320F28377D
Tool/software:
Hi Champ,
I am asking for my customer.
They are seeing a reset occurred in run-time, asking for details about under what circumstances will be established, to help on troubleshooting.
When reset occurred, they have seen the bit 15.14.11.10.9.8 in the Boot Status Bit Fields are raised.
(1). What does the bit 11 (Boot ROM handled all the resets) in Boot Status meaning ? Under what circumstances will have the bit be set ?
(2). Looking to all the bits (15.14.11.10.9.8), any bit is related to a reset ?
(3). Any error register could check for the reset source ?
Thanks and regards,
Johnny