Part Number: LAUNCHXL-F28379D
Tool/software:
Hello team,
I am working on a ADC sampling code and i wanted to transmit the adc value over CAN. I am using a basic code, basically the boot start code. I read the value of ADCIN 14 in a variable and i want to transmit the variable over can, i am not able to do so. I need any changes or linking i need to do to achieve so.
Any support will be highly appreciated.
//
// Included Files
//
#include <stdint.h>
#include <stdbool.h>
#include <stdio.h>
#include <file.h>
#include "F28x_Project.h" // DSP28x Headerfile
#include "ti_ascii.h"
#include "sci_io.h"
//
// Defines
//
//
// Micro-seconds to wait for ADC conversion. Longer than necessary.
//
#define CONV_WAIT 1L
#define TX_MSG_OBJ_ID 1
#define MSG_DATA_LENGTH 8
//
// Globals
//
extern void DSP28x_usDelay(Uint32 Count);
static unsigned short indexX=0;
static unsigned short indexY=0;
const unsigned char escRed[] = {0x1B, 0x5B, '3','1', 'm'};
const unsigned char escWhite[] = {0x1B, 0x5B, '3','7', 'm'};
const unsigned char escLeft[] = {0x1B, 0x5B, '3','7', 'm'};
const unsigned char pucTempString[] = "ADCIN14 Sample: ";
int16_t currentSample;
//
// sampleADC -
//
int16_t sampleADC(void)
{
int16_t sample;
//
// Force start of conversion on SOC0
//
AdcaRegs.ADCSOCFRC1.all = 0x03;
//
// Wait for end of conversion.
//
while(AdcaRegs.ADCINTFLG.bit.ADCINT1 == 0)
{
//
// Wait for ADCINT1
//
}
AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; // Clear ADCINT1
//
// Get ADC sample result from SOC0
//
sample = AdcaResultRegs.ADCRESULT1;
return(sample);
}
//
// drawTILogo -
//
void drawTILogo(void)
{
unsigned char ucChar, lastChar;
putchar('\n');
while(indexY<45)
{
if(indexY<45)
{
if(indexX<77)
{
ucChar = ti_ascii[indexY][indexX++] ;
//
// We are in the TI logo make it red
//
if(ucChar != '7' && lastChar=='7')
{
putchar(escRed[0]);
putchar(escRed[1]);
putchar(escRed[2]);
putchar(escRed[3]);
putchar(escRed[4]);
}
//
// We are in the TI logo make it red
//
if(ucChar == '7' && lastChar!='7')
{
putchar(escWhite[0]);
putchar(escWhite[1]);
putchar(escWhite[2]);
putchar(escWhite[3]);
putchar(escWhite[4]);
}
putchar(ucChar);
lastChar = ucChar;
}
else
{
ucChar = 10;
putchar(ucChar);
ucChar = 13;
putchar(ucChar);
indexX=0;
indexY++;
}
}
}
}
//
// clearTextBox -
//
void clearTextBox(void)
{
putchar(0x08);
//
// Move back 24 columns
//
putchar(0x1B);
putchar('[');
putchar('2');
putchar('6');
putchar('D');
//
// Move up 3 lines
//
putchar(0x1B);
putchar('[');
putchar('3');
putchar('A');
//
// Change to Red text
//
putchar(escRed[0]);
putchar(escRed[1]);
putchar(escRed[2]);
putchar(escRed[3]);
putchar(escRed[4]);
printf((char*)pucTempString);
//
// Move down 1 lines
//
putchar(0x1B);
putchar('[');
putchar('1');
putchar('B');
//
// Move back 20 columns
//
putchar(0x1B);
putchar('[');
putchar('2');
putchar('0');
putchar('D');
//
// Save cursor position
//
putchar(0x1B);
putchar('[');
putchar('s');
}
//
// updateDisplay -
//
void updateDisplay(void)
{
//
// Restore cursor position
//
putchar(0x1B);
putchar('[');
putchar('u');
printf("%d ", currentSample);
}
//
// scia_init - SCIA 8-bit word, baud rate 0x000F, default, 1 STOP bit,
// no parity
//
void scia_init()
{
//
// Note: Clocks were turned on to the SCIA peripheral
// in the InitSysCtrl() function
//
//
// 1 stop bit, No loopback, No parity,8 char bits, async mode,
// idle-line protocol
//
SciaRegs.SCICCR.all =0x0007;
//
// enable TX, RX, internal SCICLK, Disable RX ERR, SLEEP, TXWAKE
//
SciaRegs.SCICTL1.all =0x0003;
SciaRegs.SCICTL2.bit.TXINTENA =1;
SciaRegs.SCICTL2.bit.RXBKINTENA =1;
//
// 115200 baud @LSPCLK = 50MHz (200MHz SYSCLK)
//
SciaRegs.SCIHBAUD.all =0x0000;
SciaRegs.SCILBAUD.all =53;
SciaRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset
return;
}
//
// Main
//
void main()
{
volatile int status = 0;
uint16_t i;
volatile FILE *fid;
//
// If running from flash copy RAM only functions to RAM
//
#ifdef _FLASH
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
#endif
//
// Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2806x_SysCtrl.c file.
//
InitSysCtrl();
//
// For this example, only init the pins for the SCI-A port.
//
EALLOW;
GpioCtrlRegs.GPBMUX1.bit.GPIO42 = 3;
GpioCtrlRegs.GPBMUX1.bit.GPIO43 = 3;
GpioCtrlRegs.GPBGMUX1.bit.GPIO42 = 3;
GpioCtrlRegs.GPBGMUX1.bit.GPIO43 = 3;
EDIS;
//
// Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
//
DINT;
//
// Initialize PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2837xD_PieCtrl.c file.
//
InitPieCtrl();
//
// Disable CPU interrupts and clear all CPU interrupt flags
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2837xD_DefaultIsr.c.
// This function is found in F2837xD_PieVect.c.
//
InitPieVectTable();
//
// Initialize SCIA
//
scia_init();
//
// Initialize GPIOs for the LEDs and turn them off
//
EALLOW;
GpioCtrlRegs.GPADIR.bit.GPIO31 = 1;
GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1;
GpioDataRegs.GPADAT.bit.GPIO31 = 1;
GpioDataRegs.GPBDAT.bit.GPIO34 = 1;
EDIS;
//
// Enable global Interrupts and higher priority real-time debug events:
//
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
//
// Configure the ADC: Initialize the ADC
//
EALLOW;
//
// write configurations
//
AdcaRegs.ADCCTL2.bit.PRESCALE = 6; // set ADCCLK divider to /4
AdcbRegs.ADCCTL2.bit.PRESCALE = 6; // set ADCCLK divider to /4
AdcSetMode(ADC_ADCA, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE);
AdcSetMode(ADC_ADCB, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE);
//
// Set pulse positions to late
//
AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1;
AdcbRegs.ADCCTL1.bit.INTPULSEPOS = 1;
//
// power up the ADCs
//
AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1;
AdcbRegs.ADCCTL1.bit.ADCPWDNZ = 1;
//
// delay for 1ms to allow ADC time to power up
//
DELAY_US(1000);
//
// ADCA
//
EALLOW;
AdcaRegs.ADCSOC0CTL.bit.CHSEL = 0x0E; //SOC0 will convert pin ADCIN14
//
// sample window is acqps + 1 SYSCLK cycles
//
AdcaRegs.ADCSOC0CTL.bit.ACQPS = 25;
AdcaRegs.ADCSOC1CTL.bit.CHSEL = 0x0E; //SOC1 will convert pin ADCIN14
//
// sample window is acqps + 1 SYSCLK cycles
//
AdcaRegs.ADCSOC1CTL.bit.ACQPS = 25;
AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 1; //end of SOC1 will set INT1 flag
AdcaRegs.ADCINTSEL1N2.bit.INT1E = 1; //enable INT1 flag
AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //make sure INT1 flag is cleared
//
// Redirect STDOUT to SCI
//
status = add_device("scia", _SSA, SCI_open, SCI_close, SCI_read, SCI_write,
SCI_lseek, SCI_unlink, SCI_rename);
fid = fopen("scia","w");
freopen("scia:", "w", stdout);
setvbuf(stdout, NULL, _IONBF, 0);
//
// Print a TI Logo to STDOUT
//
drawTILogo();
//
// Twiddle LEDs
//
GpioDataRegs.GPADAT.bit.GPIO31 = 0;
GpioDataRegs.GPBDAT.bit.GPIO34 = 1;
for(i = 0; i < 50; i++)
{
GpioDataRegs.GPATOGGLE.bit.GPIO31 = 1;
GpioDataRegs.GPBTOGGLE.bit.GPIO34 = 1;
DELAY_US(50000);
}
//
// LEDs off
//
GpioDataRegs.GPADAT.bit.GPIO31 = 1;
GpioDataRegs.GPBDAT.bit.GPIO34 = 1;
//
// Clear out one of the text boxes so we can write more info to it
//
clearTextBox();
currentSample = sampleADC();
//
// Main program loop - continually sample temperature
//
for(;;)
{
//
// Sample ADCIN14
//
currentSample = sampleADC();
//
// Update the serial terminal output
//
updateDisplay();
//
// If the sample is above midscale light one LED
//
if(currentSample > 2048)
{
GpioDataRegs.GPBSET.bit.GPIO34 = 1;
GpioDataRegs.GPACLEAR.bit.GPIO31 = 1;
}
else
{
//
// Otherwise light the other
//
GpioDataRegs.GPBCLEAR.bit.GPIO34 = 1;
GpioDataRegs.GPASET.bit.GPIO31 = 1;
}
DELAY_US(1000000);
}
Device_init();
Device_initGPIO();
GPIO_setPinConfig(DEVICE_GPIO_CFG_CANRXB);
GPIO_setPinConfig(DEVICE_GPIO_CFG_CANTXB);
CAN_initModule(CANB_BASE);
CAN_setBitRate(CANB_BASE, DEVICE_SYSCLK_FREQ, 250000, 16);
CAN_setupMessageObject(CANB_BASE, TX_MSG_OBJ_ID, 0x181,
CAN_MSG_FRAME_STD, CAN_MSG_OBJ_TYPE_TX, 0,
CAN_MSG_OBJ_NO_FLAGS, MSG_DATA_LENGTH);
CAN_startModule(CANB_BASE);
// EINT;
while(1)
{
CAN_sendMessage(CANB_BASE, TX_MSG_OBJ_ID, MSG_DATA_LENGTH, currentSample);
while(((HWREGH(CANB_BASE + CAN_O_ES) & CAN_ES_TXOK)) == CAN_ES_TXOK)
{
}
DEVICE_DELAY_US(500000);
}
}
//
// End of File
//
Regards
Chirag