This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: Application issues.

Expert 2310 points

Part Number: TMS320F280049

Tool/software:

Hi Team,

How to configure CMPSS module? The current setting is set, but there is a change in the output PIN9,

and the CMPSS module still does not respond. What is the reason?

  • Hi Reed,

    What are you attempting to use the CMPSS to do in your application? 

    From reviewing your code briefly, I notice that you're setting the DACVAL at 1024 which corresponds to the CMPSS output high when voltage is above 3.3V / 4 = 0.825V. 

    If you are using A3, note that you must access the CMPSS through the below CMPSS module inputs

    So like 491 would not be adjusting the correct CMPSS module.

    DriverLib should look something like this

    ASysCtl_selectCMPHPMux(ASYSCTL_CMPHPMUX_SELECT_1,3U);
    Regards,
    Peter