Part Number: TMS320F28P650DK
Tool/software:

From now to 10, the CCS code is imported into the DSP, and an error message is displayed when the DSP runs. The error picture is shown as follows


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28P650DK
Tool/software:

From now to 10, the CCS code is imported into the DSP, and an error message is displayed when the DSP runs. The error picture is shown as follows


Hi,
The issue you describe is simply saying that it could not find the program to load. This usually happens when trying to debug a project where the build failed (and an executable (*.out) file was not generated). Can you please try building the project and confirm that the program is built successfully?
Best,
Matt
My program is running on CCS, loading (*.out) file, my program is generated in CCS tools according to the guide to join the corresponding process, running no error, I have a question: after this operation of the code still need to change, how to change
Hello expert, if I want to use 28p65 Ethercat as the next machine, the upper computer QT, I should use the official which process, what is the network connection, how to achieve,
Hey Nie,
The expert is out of office until tomorrow, apologies for the delayed response.
Thank you,
Luke
Hi Nie,
Are you wondering how to update the program after it's already been loaded? You'd have to re-program the new *.out file (post-changes) like before.
I'll loop in the the EtherCAT expert to address your other inquiry.
Best,
Matt
Hi Nie,
if I want to use 28p65 Ethercat as the next machine, the upper computer QT, I should use the official which process, what is the network connection, how to achieve,
If you don't have any additional questions specific to CCS, can you re-clarify this question on a new E2E thread so the relevant expert can get assigned to it?
Best,
Matt