This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Ethernet not example not working

Part Number: TMS320F28388D

Tool/software:

I am trying to get the ethernet working on the evaluation board, with the following setup:

  • F28388D controlCard on the docking station
  • Ethernet cable connected from PC to RJ45 on controlCard (J4 connector)
  • Running examples:
    • c28x - ethernet_c28x_config
    • CM - ethernet_ex2_phy_loopback
  • I am using wireshark to capture the packets

I do not see any packets from the microcontroller.

Assuming the phy-loopback example relies on external loopback, I am expecting packets to show up on the external RJ45 interface,
and hence to show up on the wireshark trace.

Any suggestions..??