Part Number: TMS320F28386D
Other Parts Discussed in Thread: UNIFLASH, SYSCONFIG
Tool/software:
My attempts to secure my device by configuring the DCSM using the Uniflash tool are failing and rendering my device inoperable.
The configuration basically consists in setting
- Final zone select block
- Zx-LINKPOINTER = 0x0 (final security configuration)
- C1 flash sectors 0, 1, 2, 3 and 4 to be in zone 1. I'm in boot from flash mode (default boot at 0x80000) and this is where the system boots from
- CM flash sectors 0, 1, 2, 3 and 4 to be in zone 1. CM also boots from flash in these sectors (0x200000) after C1 releases it.
- All other flash sectors unsecured
- All other memories unsecured
- Disable unlocking of JTAG, CSM1, CMS2
- Z1JTAGPSWDH and Z1JTAGPSWDL = 0x0 (disable JTAG password)
- JTAGLOCK (Z1OTP_JLM_ENABLE w) = 0xFFFF0000 (enable JTAG Lock module)
- Disable unlocking of CSM1 (CSM1 password is all zeros)
- Disable unlocking of CSM2 (CMS2 password is all zeros)
- Z1-PSWDLOCK = 0xFB7FFFF0
- Z2-PSWDLOCK = 0x1F7FFFF0
To apply these settings, I tried
- setting the configuration by hitting "Program Zone 2" followed by "Program Zone 1" but that didn't work. "Program Zone 2" failed midsequence leaving my device in a unJTAGable state.
- creating a Standalone CLI with my settings and applying that to a fresh device. The device was flashed with the images specified but none of the security settings were applied.
- creating a Standalone CLI with my settings only and applying that to a fresh device but nothing happened and I got a message saying that there was nothing to do.x
Am I using the correct tools to do what I'm trying to do?
Thanks,
Benjamin