This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800157: Getting a parsing error for a cfg file when trying to run debug in CCS

Part Number: TMS320F2800157

Tool/software:

I am trying to download and run my build and I get this error. 


  • Hi,

    Our expert is currently unavailable. Please expect delay of 2-3 days in the response.

    Regards,

    Divyansh

  • Hi David,

    Can you provide some more details regarding the parsing error that you are seeing? 

    Are you currently running a custom project or one of our provided example projects from the SDK? Can you view the .ccxml file and verify that it is correctly configured for your device (assuming the TMS320F2800157 based on your post)? What message do you get when you use the Test Connection button in the target configuration GUI?

    Regards,

    Peter

  • Thanks.  I was able to resolve this issue by updating my CCS.  I did have to modify the ccxml file to use the 2 pin cjtag for the _LAUNCHXL_F2800157 and the xds110 FW on the launchpad as well.  I am working through another issue now with the SysCtl_delay not showing in memory correctly.  I was looking at some forums on this and will try them.  Thanks for the help.