Other Parts Discussed in Thread: TIDA-010933
Tool/software:
Dear TI experts:
Happy New Year!
It is more urgent, please answer the questions consulted above, thank you!
Best Regards!
larry li
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Dear TI experts:
Happy New Year!
It is more urgent, please answer the questions consulted above, thank you!
Best Regards!
larry li
Part Number: TIDM-SOLARUINV
Tool/software:
Dear TI experts!
For a few questions about the inverter solution selection, TI's experts please kindly to give us guidance:
1)1KW output power,
2) Battery: 12V, 100A (discharged), 50A (charged)
3)MPPT 600w (18V-56V)
3.Is the circuit logic of TIDA-010933 MPPT like this?
SW comes out directly to the PCS and the battery, directly on the same bus, or need to add a management circuit?
4.Is there a design file in PADS or cadence or AD format for TIDA-010933 Schematic?
36V(15V-60V) step-down to 12V MPPT scheme, what is the recommended scheme for TI?
7.If we want to reduce costs, which parts must be retained, and which peripheral devices can be considered to be replaced, so that we can use the SDK software provided by TI
Best Regards!
Larry li
Dear TI experts!
Our product needs,
1. The battery needs to charge and discharge management, and it can be trickle-charged, constant-current charged, and constant-voltage charged according to the state of the battery.
2. Over-current, over-voltage, under-current, under-voltage, and short-circuit protection are required
The currently recommended reference scheme, especially the SDK,whether the software has a corresponding exception handling mechanism
Part Number: TIDM-SOLARUINV
Tool/software:
Dear TI's experts:
Continuing with the above question, for the 1KW and 5KW product requirements that we currently need to design,
Our product needs,
1. The product solution needs to realize the charging and discharging management of the battery, and can carry out trickle charging, constant current charging and constant voltage charging according to the state of the battery. Is it possible to use a single TI 280039 to communicate with the BMS for RS485/CAN, and does the SDK have this function?
2. Over-current, over-voltage, and short-circuit protection are required
The recommended reference schemes, especially whether the SDK and reference software have the corresponding exception handling mechanism
3. If 2~3 inverters are to be paralleled, what kind of solution does TI recommend to achieve it? Does TI have a corresponding parallel synchronization and power allocation control mechanism, and has it been implemented on the SDK?
4. Charging priority management, what kind of circuit scheme is recommended, and help recommend TI scheme
5. To improve the dynamic response of the load, in addition to the redundancy of reserved power devices, does TI's SDK adopt the corresponding processing method in terms of software? What is the performance achieved so far?
6. Whether TIDA-010933's current reference design SDK of TI supports the grid-connected function
Best Regards!
Larry li
TIDA-010933 is the closest to the need. Only ref design available at this time.
TIDA-010933 MPPT has boost circuits. Pls see the associated doc.
SW comes out directly to the PCS and the battery, directly on the same bus, or need to add a management circuit? This question is not clear. The s/w is available in C2000 DP SDK folder.
Design files are avalable inside the folder in C2000 DP SDK where TIDA--010933 is saved.
36V(15V-60V) step-down to 12V MPPT scheme, what is the recommended scheme for TI? Use the DC/DC buck converter for this.
We dont do detail cost analysis. Pls do your own cost assessment
Thanks Shamin for the reply!
A few more questions:
1. Paralleling: Does TI have a solution for inverter parallelism management to realize the synchronization and power balance distribution of master-slave machines after paralleling?
2. MPPT: Please kindlly recommend TI's 600W step-down MPPT, and TI 280039 reference software support that MPPT
3.Is there a design file in PADS or cadence or AD format for TIDA-010933 Schematic?