This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P650DH: Syscfg generate the configuration code even when the settings are defaut.

Part Number: TMS320F28P650DH

Tool/software:

Hi Experts,

My customer is using syscfg to generate codes that initialize the device. When syscfg generate the initialization codes, it does not generate codes for settings that is default. This would work under the assumption that these registers are untouched after reset and remains default value.

However, in my customer's use case, they would run diagnosis codes before initializing the application. The value in some registers no longer has default value. and the above assumption breaks.

Is there any way to let syscfg generates the initialization codes even when the settings are default. 

Noted that this is different to generate codes for ALL settings, in this case the code would be too large. 

Regards,

Hang.