Part Number: TMS320F28335
Tool/software:
TI's experts:
Hello!
I am a new user of 28335 and I have been having some problems with the system clock section recently.
If I am using an external oscillator connected to the XCLKIN pin and not using an on-chip oscillator, do I need to write this in code? Because I saw in the 2803 x series chips related instructions are included in the routine, such as SysCtrlRegs. CLKCTL. Bit. XCLKINOFF = 1; // Turn off XCLKIN
Does it need to be written like this in 28335?
The second question is when configuring the frequency division and frequency doubling factor, I want to adjust the frequency division factor to 1. Can I adjust the frequency division factor to 1 only when the PLL is bypassed or turned off?
Thank you!