This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800156-Q1: Frequency

Part Number: TMS320F2800156-Q1

Tool/software:

hi team,

the frequency of F2800156 is 100MHz , which is lower than other F28015X series. Could u kindly help to tell the reason?

Will there be some risks when setting the frequency of F2800156 to 120MHz? Thanks!

  • Hello Zoey,

    There are several F280015x devices with this frequency as noted in the device datasheet:

    It would not be recommended to operate the device out of datasheet specification as it has not been tested/we cannot guarantee the performance out of spec.

    Best Regards,

    Allison