Part Number: TMS320F2808
Tool/software:
Hi All,
I have a question about the C2prog setup.
I want to write to F2808 with C2Prog via RS232, but it fails.
1,C2Prog is connected to XCLKIN(Pin 90) with a crystal oscillator(16.3840MHz or 16.5888MHz) directly.
2,SCI-A Boot mode is used to start up.
3,Using .out file output from CCS
4,Tried all frequencies as there was no 16MHz option.
Only at 24MHz did it proceed to Connection for stage #1 and then the process aborted.


At other frequencies, I get autobaud failed.

Is there any way to set it up at 16MHz?
Any other solutions?
Best Regards,
Ito