Part Number: C2000WARE-MOTORCONTROL-SDK
Other Parts Discussed in Thread: TIDM-1010, C2000WARE, TMDXIDDK379D
Tool/software:
Hi, i am revisiting this topic as it is 5 years old. I am in the exact same situation as the OP. BLDC 24 pole motor and 20 bit optical encoder with SSi / BiSS-C communication. Only i am trying to get 2 axis gimbal with precision under 1 arcmin. What product would you recommend as test platform. We will be building our custom board after the test phase. It should be 48 V nominal voltage with nominal current around 2A.
Is the Insta spin still in use or is it Motor Control.
I am considering TI instead of Trinamic because of the 16 bit limit.
Thank you
Best regards
Ing. Jiri Chytil