Part Number: TMS320F2800157
Other Parts Discussed in Thread: DRV8353
Tool/software:
Hello Team,
Hello Team,
Customized PCB F2800157 integrated with UMC code(latest SDK_2.0.0) and tested with 48V(ABI-encoder).
When try to run the motor ,most of the time its successful able to achieve expected speed as per set speed.
Some rare cases motor runs at uncontrollable maximum speed.
Same kind of issues we are facing with Launchpad-F2800157 with DRV8353 (Some rare cases motor runs at uncontrollable maximum speed)
We checked the Customized PCB with #BL2 , BL#3 ,BL#4 all settings(Encoder connection) and configurations are correct.
Its clearly shows issues in encoder offset calibration.
1)How to do encoder offset calibration of a motor .
2)Is there anything need to check at #BL2 & BL#3 ?for Encoder offset calibration .
Thanks in Advance.
Regards
C.Prabhakaran