Part Number: TMS320F28388D
Tool/software:
Greetings,
I have created a simple CLA task which only executes MSTOP. I am trying to run it by using the Software start in the MIFRC register. I can see the task interrupt pending in MIFR, but it never executes. The CLA’s PC is 0x0000. Things such as the PIE and LSx RAMs which use CPU1.SYSCLK are working. And CpuSysRegs.PCLKCR0.CLA1 is 1. So the CLA should be getting a clock. The vectors in MVECTx are correct, and the machine code at the vector address for the task being started is also correct for the MSTOP instruction. Is there something else which needs to be setup?
Thank you,
Ed