Hello TI-community,
We are using TMS320C2000 development tools with TMS320F28335PGFA and CCS 4.2.4 to test SCI-A port in tx and in rx. We are testing Example_2833xSci_Echoback. The tx from device to PC is ok, but the tx from PC to device doesn't work. We have read that we should switch in the "On" position the controlCARD SW1, that is currently in the "Off" position. Is this a possible solution for solve our problem?
We have other two questions:
1) If we switch in the "on" position the controlCARD SW1, is there the risk to damage the device?
2) If we switch in the "on" position the controlCARD SW1, does the USB JTAG XDS100 still work for communication and diagnostic?
thanks,
Greatings