Part Number: TMS320F28379D
Tool/software:
Hello experts ,
Can you please tell me the actual value of QCLK which is the Unit position event frequency clock in (MHz)
Looking into the driverlib function "EQEP_setCaptureConfig" description:
//***************************************************************************** // //! Configures eQEP module edge-capture unit. //! //! \param base is the base address of the eQEP module. //! \param capPrescale is the prescaler setting of the eQEP capture timer clk. //! \param evntPrescale is the prescaler setting of the unit position event //! frequency. //! //! This function configures the operation of the eQEP module edge-capture //! unit. The \e capPrescale parameter provides the configuration of the eQEP //! capture timer clock rate. It determines by which power of 2 between 1 and //! 128 inclusive SYSCLKOUT is divided. The macros for this parameter are in //! the format of EQEP_CAPTURE_CLK_DIV_X, where X is the divide value. For //! example, \b EQEP_CAPTURE_CLK_DIV_32 will give a capture timer clock //! frequency that is SYSCLKOUT/32. //! //! The \e evntPrescale parameter determines how frequently a unit position //! event occurs. The macro that can be passed this parameter is in the format //! EQEP_UNIT_POS_EVNT_DIV_X, where X is the number of quadrature clock //! periods between unit position events. For example, //! \b EQEP_UNIT_POS_EVNT_DIV_16 will result in a unit position event //! frequency of QCLK/16. //! //! \return None. // //*****************************************************************************
In the last line it says "For example, EQEP_UNIT_POS_EVNT_DIV_16 will result in a unit position event
frequency of QCLK/16."
But what is QCLK in the first place?
If i configure the function like this:
EQEP_setCaptureConfig(obj->qepHandle, EQEP_CAPTURE_CLK_DIV_128, EQEP_UNIT_POS_EVNT_DIV_32);
The capture timer clock will be SYSCLKOUT/128, if the system clock is 200 MHz, then this would be 200/128 = 1.56 MHz.
But what would the Unit position event frequency be?
Looking into the TRM i found this , but it dosn't help be calculate the value of QCLK.(unless it means 4 * 200 / 32 = 25 MHz?)

Kindly help!