Part Number: F29H85X-SOM-EVM
Other Parts Discussed in Thread: HSEC180ADAPEVM, TMDSHSECDOCK, , SYSCONFIG
Tool/software:
Hi team,
I'm using the F29H85X-SOM-EVM, connected to the HSEC180ADAPEVM, connected to the TMDSHSECDOCK.
I am running the adc_ex2_soc_epwm example.
When I run the example with SOC0 channel set to single-ended, ADCIN0, and connect ANA 9 of the TMDSHSECDOCK to 3.3 V I get the correct value in the watch expression window, which means the code is working.

I then change the channel to channel 6 in sysconfig, rebuild and load the project. I connected ANA 25 of the board to 3.3V.
I get unknown data on the input side. Am I using the wrong pin, or is there some other setting that I need to change to get ADC channel 6 to produce the correct data?

Thanks Team?