Other Parts Discussed in Thread: LAUNCHXL-F280039C, , TIDM-DC-DC-BUCK
Tool/software:
Hello,
We are working with the TMS320F280039C MCU and using the CMPSS trip function to disable the PWM in the event of an overcurrent. We have both the 'LAUNCHXL-F280039C' and the 'F280039C control card'. The code works perfectly on the Launchpad but shows deviations from the actual tripping set point on the control card. Currently, we are unsure why the trip event produced by the same F280039C on the Launchpad differs from that on the control card. We are using the 'TIDM-DC-DC-BUCK' firmware as the base code for the TMS320F280039C microcontroller.
Thanks & Regards,
Prathamesh.