This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SCI bus timeout interrupt?



Hello,

I am working with the 320F28335-HT. I have written my Sci driver but was wondering if there is any way to invoke the RX interrupt through a timeout without using another CPU timer.

Basically, I have my FIFO set up to cause the interrupt after the buffer has a minumum of 8 words. If the FIFO only contains 4 words, the interrupt won't fire. Is there anyway to invoke the RX interrupt if the FIFO has less than 8 words but has not received another one after X amount of time (without a timer)?

 

 

Thank You