Other Parts Discussed in Thread: LAUNCHXL-F280049C, BOOSTXL-DRV8320RS, , C2000WARE, MOTORWARE
Tool/software:
Dear TI Support Team,
I am currently working with a custom board that utilizes the TMS320F280049C and DRV8320RS chips. Initially, I tested the BOOSTXL-DRV8320RS BoosterPack mounted on the LAUNCHXL-F280049C LaunchPad development kit. Using this setup:
- I ran Lab05 to determine the motor parameters.
- I ran Lab09 to test the maximum motor speed, which reached 920 Hz. At this speed, while there was some fluctuation, the motor remained stable without any alarming issues.
Recently, I transitioned to a self-designed custom board where I made the following modifications:
- Adjusted some resistors affecting
USER_ADC_FULL_SCALE_VOLTAGE_Vand recalculated as follows: - Changed the shunt resistor (
R_shunt) and updated related calculations: - Adjusted the voltage filter pole:
I ran Lab02 on the custom board to obtain new offset values and verified them by running Lab05 to retrieve the motor parameters, which were similar to the original setup.
However, when I ran Lab09 to test the motor’s maximum speed:
- The motor became unstable at 850 Hz.
- The power supply exhibited abnormal behavior with high current draw and significant voltage drops.
- The motor produced strange noises during operation.
In contrast, with your board, the motor could reach its maximum speed without these issues. While oscillations occurred at the maximum speed, the power supply remained stable.
Could you please help me identify potential causes for the instability on my custom board? Any advice or guidance would be greatly appreciated.
Thank you for your time and support.
Best regards,
Hyu