Part Number: TMS320F28388D
Other Parts Discussed in Thread: SYSCONFIG, , C2000WARE
Tool/software:
Hi,
I am developing a product using a TMS320F28388D, using Sysconfig for the peripheral configuration. One of the converters is a phase-shifted full bridge, so I am looking at HRPWM configuration with phase regulation.
The program works without HRPWM activated. However, when HRPWM is activated in sysconfig, the PWMs are no longer synchronized.
I believe the configuration is correct :


And yet, no synchronisation of the 2 ePWMs.
Upon investigation, I found that the should-be-sync-ed ePWM has his EPwmXRegs.TBCTL.PHSEN = 0.
Looking at the code generated by Sysconfig, I have the HR phase enabled twice, but the regular phase is not enabled :

If I add the "normal phase" enable somewhere manually :
This line causes EPwmXRegs.TBCTL.PHSEN = 1. Then the ePWMs are sync-ed.
I am under the impression that when HRPWM and HR phase are enabled, the box for phase enabling is mis-translated into the HRPWM_ function rather than the EPWM_ function. Which causes the issue with synchronisation of the ePWMs.
Best regards,
Adrien