This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: C2000Ware Digital Power SDK 5.03.00.00 "SPLL_3PH_DDSRF"

Part Number: TMS320F28388D

Tool/software:

Dear Sir/Madam,

We are using this 3 phase SPLL to get the frequency. We found the setting time requires more than 10 grid cycles(200ms in a 50Hz grid). The settling time is a concern for me. Do you have any idea?

We are using the procedure as suggested by the SDK document:

SPLL_3ph_DDSRF_init(AC_FREQ_HZ,
(float32_t)(1.0 / ISR1_FREQUENCY_HZ),
(float32_t)(0.00188141f),
(float32_t)(-0.99623717f),
&spll_3ph_1);
spll_3ph_1.lpf_coeff.b0 = 333.807f;
spll_3ph_1.lpf_coeff.b1 = -333.674f;
Our simulation sampling frequency is 6.4kHz. 
The b0, b1 are used exactly as above. We also try different values as per "Software Phase Locked Loop Design Using C2000Tm Microcontrollers *.pdf"
for example,
const float32_t k_K1 = 0.004885f;
const float32_t k_K2 = -0.99023f;
const float32_t k_3PH_LPF_B0 = 266.6772959f;
const float32_t k_3PH_LPF_B1 = -266.656037f;
Thanks