Part Number: TMS320F28379S
Tool/software:
Hello,
I have a question about DCSM usage and JTag connection.
I'm studying DCSM through the project Import in CCS using dscm_security_tool.syscfg.
The configuration settings are as follows:
Flash A~H Sector - Lock
RAM LS0~4 - Lock
Password(CSMPSWD0~3) - My desired value
Boot Mode - Flash
PSWDLOCK - Final Lock
Questions:
1. Although it operates with Flash execution Code, the PWM Interrupt is copied to RAM.
In this case, since it's protected by GRABRAM rather than EXEONLYRAM, will the Code in the RAM area operate normally?
2. After executing steps 1-4 above, I set the PSWDLOCK.
How do I connect JTag after this?
The syscfg tool doesn't support Other(Wait/Flash) in Get Mode.
In the attached image, it's also selected as Flash Boot.
Should I use Wait Boot instead?
Have a great weekend~!