This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I am a beginner with C2000 series and not familiar with command file.
My code was checked In RAM mode.
My project is configured by sysconfig tool and command file is also created by sysconfig.
What I need is that code is saved to flash memory and copied to RAM for execution.
Hi Yoonsun,
Please have a look at similar thread of copying contents from FLASH to RAM -
Also please have a look at the "Flash to RAM Project ex3" example in the SDK for a different device for better clarity - C2000Ware_5_04_00_00\driverlib\f2838x\examples\c28x\flash
Thanks
Aswin