On the TMS320F28035 datasheet, TMS and TDI are not pulled-up. But this document -> http://www.google.com/url?sa=t&rct=j&q=error%20connecting%20to%20the%20target%3Aerror%200x00001200%2F-1041&source=web&cd=1&ved=0CBsQFjAA&url=http%3A%2F%2Fe2e.ti.com%2Fcfs-filesystemfile.ashx%2F__key%2FCommunityServer.Components.PostAttachments%2F00.00.13.90.84%2FI-am-trying-to-connect-to-an-TMS320F2812-with-an-XDS100v2-emulator.pdf&ei=bKa9Tq73McHj0QHd2_GtBA&usg=AFQjCNGE7FXC--N9uQbMyurdWHIA1EBR2Q said otherwise. Which one is correct?
I'm getting the same error as mentioned in the PDF.
Also, regarding the pin layout on XDS100v2 JTAG header, which one is correct?
1 2
3 4
5 6 <-- blocked, KEY
7 8
9 10
11 12
Or
1 14
2 13
3 12 <-- blocked
4 11
5 10
6 9
7 8
Thanks