This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: Same Compiler with different compilation warning

Part Number: TMS320F280039C
Other Parts Discussed in Thread: C2000WARE

Tool/software:

Hi Champ,

I am asking for my customer.

They are using compiler v22.6.1.LTS with F280039C. They encounter with the same compiler version, but compile the project in different PCs, the compilation warning is different.

In PC 1, the warning is shown as below.

  (PC 1)

In PC 2, the warning is shown as below.

  (PC 2)

(1). Two PCs are using the same version of compiler. Any reason / setting in the properties causing the different compilation warning ?

(2). The fourth warning " Statement has no effect ‘CPUtoCLA.max_period_set_45k_flag == 0 " didn't show up in PC 2 that had a concern from customer about our compiler, any fix on this ?

Thanks for the expert's input.

Regards,

Johnny

  • Hello,

    I brought this thread to the attention of the compiler experts for further assistance.

    Thanks

    ki

  • There is some configuration issue related to the version of the C2000Ware_DigitalPower_SDK.  That needs to be cleared up first.  I'm not sure of the best thing to do. Upgrade to the latest one?  Revert back to an earlier version that worked before?  Once that question is settled, both PCs should implement the same solution.  I suspect many problems will go away after that.  Then we can deal with whatever is left.

    Thanks and regards,

    -George