Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Tool/software:
I've been working with the TMS320F2837xx & 2838xx parts for about two years. Now that we have a custom board that doesn't have a lot of test points I thought that it would be useful to try the GPIO mirroring via the XBar functionality. 
I thought it'd be easy to start with the External Interrupts example (C2000Ware_5_00_00_00\device_support\f2837xd\examples\cpu1\external_interrupt) from the C2000Ware v5.00.00. Not so fast!
I added in the required couple header files & lines of configuration code & nothing! What am I missing. I've seen other posts that make it seem simple, I can not get it to work.
I'm also using the TMDSHSEDOCK v6.0 & the f28379D controlCard rev 1.3.
I've included the example code.
So much for straight forward ;)