This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Copy some functions from flash to read

Part Number: TMS320F28379D

Tool/software:

Hi,

I am using TMS320F28379D 176 pin controller. I want to load my code in flash. But I want to execute some function from RAM. So at power up I need to copy that functions from FLASH to RAM. Please find attached file for the reference of .cmd file I am using. I have added attributes to the functions which needed to be execute from RAM. e.g.

#pragma CODE_SECTION(Read_EEPROM, ".TI.ramfuncs")
    void Read_EEPROM(uint16_t,uint8_t *,uint8_t);

//=========== .cmd File ================//


MEMORY
{
PAGE 0 :  /* Program Memory */
          /* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
          /* BEGIN is used for the "boot to Flash" bootloader mode   */

   BEGIN               : origin = 0x080000, length = 0x000002
   RAMM0               : origin = 0x000123, length = 0x0002DD
   RAMD0               : origin = 0x00B000, length = 0x000800
   RAMLS0              : origin = 0x008000, length = 0x000800
   RAMLS1              : origin = 0x008800, length = 0x000800
   RAMLS2              : origin = 0x009000, length = 0x000800
   RAMLS3              : origin = 0x009800, length = 0x000800
   RAMLS4              : origin = 0x00A000, length = 0x000800
   RAMGS14          : origin = 0x01A000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   RAMGS15          : origin = 0x01B000, length = 0x000FF8     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */

//   RAMGS15_RSVD     : origin = 0x01BFF8, length = 0x000008    /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

   RESET               : origin = 0x3FFFC0, length = 0x000002

   /* Flash sectors */
   FLASHA           : origin = 0x080002, length = 0x001FFE    /* on-chip Flash */
   FLASHB           : origin = 0x082000, length = 0x002000    /* on-chip Flash */
   FLASHC           : origin = 0x084000, length = 0x002000    /* on-chip Flash */
   FLASHD           : origin = 0x086000, length = 0x002000    /* on-chip Flash */
   FLASHE           : origin = 0x088000, length = 0x008000    /* on-chip Flash */
   FLASHF           : origin = 0x090000, length = 0x008000    /* on-chip Flash */
   FLASHG           : origin = 0x098000, length = 0x008000    /* on-chip Flash */
   FLASHH           : origin = 0x0A0000, length = 0x008000    /* on-chip Flash */
   FLASHI           : origin = 0x0A8000, length = 0x008000    /* on-chip Flash */
   FLASHJ           : origin = 0x0B0000, length = 0x008000    /* on-chip Flash */
   FLASHK           : origin = 0x0B8000, length = 0x002000    /* on-chip Flash */
   FLASHL           : origin = 0x0BA000, length = 0x002000    /* on-chip Flash */
   FLASHM           : origin = 0x0BC000, length = 0x002000    /* on-chip Flash */
   FLASHN           : origin = 0x0BE000, length = 0x001FF0    /* on-chip Flash */

//   FLASHN_RSVD     : origin = 0x0BFFF0, length = 0x000010    /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

PAGE 1 : /* Data Memory */
         /* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */

   BOOT_RSVD       : origin = 0x000002, length = 0x000121     /* Part of M0, BOOT rom will use this for stack */
   RAMM1           : origin = 0x000400, length = 0x0003F8     /* on-chip RAM block M1 */
//   RAMM1_RSVD      : origin = 0x0007F8, length = 0x000008     /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
   RAMD1           : origin = 0x00B800, length = 0x000800

   RAMLS5      : origin = 0x00A800, length = 0x000800

   RAMGS0      : origin = 0x00C000, length = 0x001000
   RAMGS1      : origin = 0x00D000, length = 0x001000
   RAMGS2      : origin = 0x00E000, length = 0x001000
   RAMGS3      : origin = 0x00F000, length = 0x001000
   RAMGS4      : origin = 0x010000, length = 0x001000
   RAMGS5      : origin = 0x011000, length = 0x001000
   RAMGS6      : origin = 0x012000, length = 0x001000
   RAMGS7      : origin = 0x013000, length = 0x001000
   RAMGS8      : origin = 0x014000, length = 0x001000
   RAMGS9      : origin = 0x015000, length = 0x001000
   RAMGS10     : origin = 0x016000, length = 0x001000

//   RAMGS11     : origin = 0x017000, length = 0x000FF8   /* Uncomment for F28374D, F28376D devices */

//   RAMGS11_RSVD : origin = 0x017FF8, length = 0x000008    /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

   RAMGS11     : origin = 0x017000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   RAMGS12     : origin = 0x018000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   RAMGS13     : origin = 0x019000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */

   CPU2TOCPU1RAM   : origin = 0x03F800, length = 0x000400
   CPU1TOCPU2RAM   : origin = 0x03FC00, length = 0x000400
}

SECTIONS
{
   /* Allocate program areas: */
   .cinit              : > FLASHB      PAGE = 0, ALIGN(8)
   .text               : >> FLASHB | FLASHC | FLASHD | FLASHE      PAGE = 0, ALIGN(8)
   codestart           : > BEGIN       PAGE = 0, ALIGN(8)
   /* Allocate uninitalized data sections: */
   .stack              : > RAMM1       PAGE = 1
   .switch             : > FLASHB      PAGE = 0, ALIGN(8)
   .reset              : > RESET,      PAGE = 0, TYPE = DSECT /* not used, */

#if defined(__TI_EABI__)
   .init_array         : > FLASHB,       PAGE = 0,       ALIGN(8)
   .bss                : > RAMLS5,       PAGE = 1
   .bss:output         : > RAMLS3,       PAGE = 0
   .bss:cio            : > RAMLS5,       PAGE = 1
   .data               : > RAMLS5,       PAGE = 1
   .sysmem             : > RAMLS5,       PAGE = 1
   /* Initalized sections go in Flash */
   .const              : > FLASHF,       PAGE = 0,       ALIGN(8)
#else
   .pinit              : > FLASHB,       PAGE = 0,       ALIGN(8)
   .ebss               : >> RAMLS5 | RAMGS0 | RAMGS1,    PAGE = 1
   .esysmem            : > RAMLS5,       PAGE = 1
   .cio                : > RAMLS5,       PAGE = 1
   /* Initalized sections go in Flash */
   .econst             : >> FLASHF      PAGE = 0, ALIGN(8)
#endif

   Filter_RegsFile     : > RAMGS0,       PAGE = 1

   SHARERAMGS0        : > RAMGS0,        PAGE = 1
   SHARERAMGS1        : > RAMGS1,        PAGE = 1
   SHARERAMGS2        : > RAMGS2,        PAGE = 1
   ramgs0           : > RAMGS0,     PAGE = 1
   ramgs1           : > RAMGS1,     PAGE = 1

#ifdef __TI_COMPILER_VERSION__
    #if __TI_COMPILER_VERSION__ >= 15009000
        #if defined(__TI_EABI__)
            .TI.ramfunc : {} LOAD = FLASHD,
                                 RUN = RAMLS0,
                                 LOAD_START(RamfuncsLoadStart),
                                 LOAD_SIZE(RamfuncsLoadSize),
                                 LOAD_END(RamfuncsLoadEnd),
                                 RUN_START(RamfuncsRunStart),
                                 RUN_SIZE(RamfuncsRunSize),
                                 RUN_END(RamfuncsRunEnd),
                                 PAGE = 0, ALIGN(8)
        #else
            .TI.ramfunc : {} LOAD = FLASHD,
                             RUN = RAMLS0,
                             LOAD_START(_RamfuncsLoadStart),
                             LOAD_SIZE(_RamfuncsLoadSize),
                             LOAD_END(_RamfuncsLoadEnd),
                             RUN_START(_RamfuncsRunStart),
                             RUN_SIZE(_RamfuncsRunSize),
                             RUN_END(_RamfuncsRunEnd),
                             PAGE = 0, ALIGN(8)
        #endif
    #else
   ramfuncs            : LOAD = FLASHD,
                         RUN = RAMLS0,
                         LOAD_START(_RamfuncsLoadStart),
                         LOAD_SIZE(_RamfuncsLoadSize),
                         LOAD_END(_RamfuncsLoadEnd),
                         RUN_START(_RamfuncsRunStart),
                         RUN_SIZE(_RamfuncsRunSize),
                         RUN_END(_RamfuncsRunEnd),
                         PAGE = 0, ALIGN(8)
    #endif

#endif

   /* The following section definitions are required when using the IPC API Drivers */
    GROUP : > CPU1TOCPU2RAM, PAGE = 1
    {
        PUTBUFFER
        PUTWRITEIDX
        GETREADIDX
    }

    GROUP : > CPU2TOCPU1RAM, PAGE = 1
    {
        GETBUFFER :    TYPE = DSECT
        GETWRITEIDX :  TYPE = DSECT
        PUTREADIDX :   TYPE = DSECT
    }

   /* The following section definition are for SDFM examples */
   Filter1_RegsFile : > RAMGS1,    PAGE = 1, fill=0x1111
   Filter2_RegsFile : > RAMGS2,    PAGE = 1, fill=0x2222
   Filter3_RegsFile : > RAMGS3,    PAGE = 1, fill=0x3333
   Filter4_RegsFile : > RAMGS4,    PAGE = 1, fill=0x4444
   Difference_RegsFile : >RAMGS5,     PAGE = 1, fill=0x3333
}

/*
//===========================================================================
// End of file.
//===========================================================================
*/

//===================================//

When I am using this function in while its execution time is almost same as executed from FLASH.

It should give faster response. I have observed it on clock pin of I2C. I2C is executed using GPIO.

Let me know what I am missing to copy this function to RAM?

Thanks,

Dhaval