Part Number: LAUNCHXL-F280049C
Other Parts Discussed in Thread: AM67A
Tool/software:
When I connect the LAUNCHXL-F280049C board to my computer, it no longer shows up in Windows Device Manager.
When I start Code Composer Studio (Version: 20.0.1.4__1.6.1) up, I get the following error message:
"No compatible board detected - please connect your board"
I have tried to run xdsdfu.exe after resetting the board by connecting pin 97 of TM4C129 to GND under power up and installed XDS110 (Version: 3.0.0.31) with xdsdfu.exe. But when I start up CCS (Version: 20.0.1.4__1.6.1) up, it immediately force an installation of XDS110 (Version: 3.0.0.33). So next time I connect the USB cable to the computer, it is again not visible in Windows Device Manager.
I have discovered that if I press the switch marked "S1 XRsn" on the LAUNCHXL-F280049C board just before I insert the USB cable into the computer and then release switch after I have inserted the USB cable, the board now shows up in Windows Device Manager and I can work with the board. But I have spent an entire day researching the problem before I found this intermediate solution.
Before, the board always showed immediately after being connected with the USB cable without having to do anything special.
Set-up information:
Windows version
===============================================================================
Edition Windows 11 Enterprise
Version 23H2
Installed on 2024-07-03
OS build 22631.4751
Experience Windows Feature Experience Pack 1000.22700.1055.0
Code Composer Studio
===============================================================================
Details
Version: 20.0.1.4__1.6.1
xdsdfu.exe
===============================================================================
PS C:\ti\ccs1271\ccs\ccs_base\common\uscif\xds110> .\xdsdfu.exe -e
USB Device Firmware Upgrade Utility
Copyright (c) 2008-2019 Texas Instruments Incorporated. All rights reserved.
Scanning USB buses for supported XDS110 devices...
<<<< Device 0 >>>>
VID: 0x0451 PID: 0xbef3
Device Name: XDS110 Embed with CMSIS-DAP
Version: 3.0.0.33
Manufacturer: Texas Instruments
Serial Num: CL491035
Mode: Runtime
Configuration: Standard
Found 1 device.