A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have the older version (V1) and
I would want to buy several TDMSPLCKIT-V3. That version doesn’t have the same
DSP (F28069) that the other one (F28335).
I want to keep the DSP F28335
because it has some difference with F28069, for example the frequency, flash… I
don't know if I can connect to the new this board. If it is pin to pin
compatible.
Also I have some AFE's that I
want to keep with the older version.
¿Could I use the TMDSPLCKIT-V3
with the F28335 without migrating the code to the F28069? ¿And the AFE?
¿Could you tell me where I can
found the schematics for this board?