Part Number: TMS320F28384S
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hi
I have imported the cla_ex4_pwm_control project in the WORKSPACE_CCSTHEIA the first time the project compile with no error. I have done some minimal modification and now I have this result:
[0]**** Build of configuration CPU1_RAM for project cla_ex4_pwm_control ****
[1]"C:\\ti\\ccs2002\\ccs\\utils\\bin\\gmake" -k -j 8 all -O
[2]Building file: "../cla_ex4_pwm_control.c"
[3]Invoking: C2000 Compiler
[4]"C:/ti/ccs2002/ccs/tools/compiler/ti-cgt-c2000_22.6.1.LTS/bin/cl2000" -v28 -ml -mt --cla_support=cla2 --float_support=fpu64 --idiv_support=idiv0 --tmu_support=tmu0 --vcu_support=vcrc -Ooff --include_path="C:/Users/lucam/workspace_ccstheia/cla_ex4_pwm_control" --include_path="C:/ti/c2000/C2000Ware_5_04_00_00" --include_path="C:/Users/lucam/workspace_ccstheia/cla_ex4_pwm_control/device" --include_path="C:/ti/c2000/C2000Ware_5_04_00_00/driverlib/f2838x/driverlib/" --include_path="C:/ti/ccs2002/ccs/tools/compiler/ti-cgt-c2000_22.6.1.LTS/include" --define=RAM --define=CPU1 --diag_suppress=10063 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --cla_background_task=off --cla_signed_compare_workaround=on --preproc_with_compile --preproc_dependency="cla_ex4_pwm_control.d_raw" --include_path="C:/Users/lucam/workspace_ccstheia/cla_ex4_pwm_control/CPU1_RAM/syscfg" --cmd_file="syscfg/board.opt" --cmd_file="syscfg/c2000ware_libraries.opt" "../cla_ex4_pwm_control.c"
[5]>> Compilation failure
[6]subdir_rules.mk:9: recipe for target 'cla_ex4_pwm_control.obj' failed
[7]"C:/ti/c2000/C2000Ware_5_04_00_00/driverlib/f2838x/driverlib/inc/hw_types.h", line 51: error #20: identifier "uint16_t" is undefined
[8]"C:/ti/c2000/C2000Ware_5_04_00_00/driverlib/f2838x/driverlib/inc/hw_types.h", line 52: error #20: identifier "int16_t" is undefined
[9]2 errors detected in the compilation of "../cla_ex4_pwm_control.c".
[10]gmake: *** [cla_ex4_pwm_control.obj] Error 1
[11]Building file: "../cla_ex4_pwm_control_cla.cla"
[12]Invoking: C2000 Compiler
[13]"C:/ti/ccs2002/ccs/tools/compiler/ti-cgt-c2000_22.6.1.LTS/bin/cl2000" -v28 -ml -mt --cla_support=cla2 --float_support=fpu64 --idiv_support=idiv0 --tmu_support=tmu0 --vcu_support=vcrc -Ooff --include_path="C:/Users/lucam/workspace_ccstheia/cla_ex4_pwm_control" --include_path="C:/ti/c2000/C2000Ware_5_04_00_00" --include_path="C:/Users/lucam/workspace_ccstheia/cla_ex4_pwm_control/device" --include_path="C:/ti/c2000/C2000Ware_5_04_00_00/driverlib/f2838x/driverlib/" --include_path="C:/ti/ccs2002/ccs/tools/compiler/ti-cgt-c2000_22.6.1.LTS/include" --define=RAM --define=CPU1 --diag_suppress=10063 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi --cla_background_task=off --cla_signed_compare_workaround=on --preproc_with_compile --preproc_dependency="cla_ex4_pwm_control_cla.d_raw" --include_path="C:/Users/lucam/workspace_ccstheia/cla_ex4_pwm_control/CPU1_RAM/syscfg" --cmd_file="syscfg/board.opt" --cmd_file="syscfg/c2000ware_libraries.opt" "../cla_ex4_pwm_control_cla.cla"
[14]>> Compilation failure
[15]subdir_rules.mk:43: recipe for target 'cla_ex4_pwm_control_cla.obj' failed
[16]"C:/ti/c2000/C2000Ware_5_04_00_00/driverlib/f2838x/driverlib/inc/hw_types.h", line 51: error #20: identifier "uint16_t" is undefined
[17]"C:/ti/c2000/C2000Ware_5_04_00_00/driverlib/f2838x/driverlib/inc/hw_types.h", line 52: error #20: identifier "int16_t" is undefined
[18]2 errors detected in the compilation of "../cla_ex4_pwm_control_cla.cla".
[19]gmake: *** [cla_ex4_pwm_control_cla.obj] Error 1
[20]gmake: Target 'all' not remade because of errors.
[21]**** Build Finished ****
what appens?
Best Regards
Luca