This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P650DK: Sysconfig MCAN board.c

Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: SYSCONFIG

Tool/software:

Hi,

I have been working on the single MCAN  (MCAN-A) with TMS320F28P650DK configured with sysconfig without problem.

Recently I tried to configure the second MCAN (MCAN-B) but it wouldn't generate the init function in board.c for seconding MCAN (MCAN-B)

After some experiments, i realized the init function of MCAN-B would not be generated if i have set "Standard Filter Elements" to any number other than 0 in "Message RAM Configuration" of MCAN-A.

Would like to check if there is issue with the sysconfig?

  • Hello Wee Khee Ho,

    Thank you for pointing this out. I will replicate this issue on my end and check with the software dev team if this behavior is expected (seems unlikely). I will follow up within the week or once more information is available.

    Best Regards,

    Zackary Fleenor