Part Number: TMS320F28069M
Other Parts Discussed in Thread: LAUNCHXL-F28069M, INSTASPINUNIVERSALGUI
Tool/software:
I'm using the LaunchXL-F28069M for a motor control project. I can use a GUI provided by TI (instaspinuniversalgui_v105.exe) to instrument the variables but can't make any changes to it as it's a binary file.
To customise the GUI, I was trying to import a GUI project into the cloud GUI designer and the closest GUI I can find from the Gallery is "C2000 InstaSPIN Universal GUI". I checked the connection configuration and make sure the device is the same as on the F28069 launchpad, i.e. "Texas Instruments XDS100v2 USB Debug Probe". But when I ran the GUI I got connection error: "... Device TMS320F2806xM is not supported". The information in the manual for the working GUI does say it is for F28049 but I thought it should at least connect as the comms device is the same?