Part Number: TMS320F28P659DH-Q1
Tool/software:
Hi,
We are using TMS320F28P659 for our custom board and we have some queries regarding the initial boot. As per the datasheet,
In our hardware, we are planning to fix flash boot mode always ( HIGH in gpio72 and gpio84) and boot mode switch is not available. Also we don't have USB peripheral in our custom HW. We have some queries on the initial boot
1. Assuming that after purchase, the chip will be in the Unprogrammed device condition and in the first time after powering ON , will we be able to flash via JTAG (flash boot mode) or only with USB mode.
2. Is there any procedure to follow during bring up of the chip for the first time after purchase (we don't have secure boot requirements)
Thanks in advance