Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: TIDM-DC-DC-BUCK, BOOSTXL-BUCKCONV, LAUNCHXL-F280049C, POWERSUITE, SFRA
Tool/software:
Hi @Peter Luong1
You had sent me this ACMC code in a previous conversation thread (shown below) a while ago. I'm looking into it now and I don't see the #define ACMC in the buck_user_settings.h file. Also I don't see the lab2_acmc.js file either.
Regards,
Mike Allette
"Hi Mike,
This zip contains the CCS project to demonstrate ACMC on the TIDM-DC-DC-BUCK project interfacing on the BOOSTXL-BUCKCONV hardware with F28004x LaunchPad. This has been fully tested on hardware but compensators are generic and not tuned. From my testing, this works as expected
ACMC is implemented on top of the closed-loop VMC build (build 2).
Project can switch between closed-loop VMC and closed-loop ACMC by changing the #define ACMC in the buck_user_settings.h file. Setting to 1 will be ACMC and setting it to 0 will be VMC.
Also, I have created a different debug environment so you can execute this script to see the desired ACMC variables used in the code. Refer to the lab2_acmc.js file
Regards,
Peter"