Part Number: TMS320F2800157
Other Parts Discussed in Thread: DRV8353
Tool/software:
Hello team,
Currently, I am working on regenerative braking using DRV8353 EVM and f2800157 launchpad.
I want support from TI experts to implement regenerative braking in the universal motor code.
Currently I am working on 24V encoder motor and we are able to run the motor in both FAST and ENCODER estimator methods and in all build levels.
I attached the motor data sheet for reference.
Can you please suggest some documents regarding regenerative braking. I want to know which sides of the MOSFETs we need to switch during this condition.
Currently we are running our motor in speed control mode. I want to know, can we able to implement regenerative braking in speed control mode or we need current control mode only (Torque control mode) ?
As I know, in universal motor code we have different types of braking.
I want to know, apart from this, anything is there, related to regenerative braking in universal motor code?
I want to implement regenerative braking in build level 4 under MOTOR1_ENC estimator.
Please suggest the way to implement this in our code.
Thank you,
Regards,
Kirana H P