Part Number: TMS320F28035
Other Parts Discussed in Thread: PMP41078
Tool/software:
Hello:
We need to use 30V input with 64V output with 6000W power, must provide a constant current , voltage variation not a substantial issue. But constant current output control with the least output capacitor are required.
Thinking the best option is GaN phase-shifted Full-Bridge ( with Synchronous rectification ) topology with output current sense & feedback to the Shunt regulator. Maybe use 4 identical modules in parallel.
In the TIDU248–May 2014 document, they use TMS320F280XX series DSP-- we might use a Delfino if possible.
Given the low input voltage, is PSFB right selection ?
Where can we find the Code for PSFB control?
Appreciate any comments/suggestions on this matter.
r