This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320

Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: C2000WARE

Tool/software:

Hi:

I need to use the TMS320F28P650DK for the following:

real time applications with input sample about 3.5 MSPS through the ADC, the input signal is a noisy periodic signal- assume sine wave- i need to lock it to an numerically controlled oscillator (NCO) programmed inside the DSP, also all other functions will be there ; PID and filters, so basically, it is a software implemented phase locked loop where everything is in the DSP realm, the frequency of the signal is between 20 KHz to 1MHz...

is TMS320F28P650DK suitable for this application?

If not, which DSP processor can perform?

it is possible to use external ADC and DAC too...

Also, frequency resolution should be around 0.005 Hz

Thanks