Part Number: TMS320F2812
Tool/software:
I'm a longtime user of CCS since v3.1 and now using CCS v6.1 for an older project. I bought a Blackhawk BH-USB560M emulator and I'm tryting to setup to use it with CCS v6.1 but can't find the Blackhawk subdir in the \emulators subdir. I tried using the CCS Install New Software utility but it failed and not sure what to do. It shouldn't be this hard to setup my Target to use a standard emulator like Blackhawk. I'm using this o na Dell M6800 laptop with Windows 10, with latest updates.
Please note that I've tested it using the non CCS Blackhawk utility called BHProbe.2 and it's connecting to my target and working fine based on receivieng no errors and passed all tests from the Blackhawk utility app.
Please advise what steps I should take or where to find the instructions to setup a Target Config using Blackhawk including downloading and installing any required Blackhawk CCS files. I've contacted Blackhawk. now Corelis support to get download access to their Blackhawk-dsp.com server that should have the files. Due to changes to their website, I can't get access unless Corelis support gives me a set of login credentials for the download site and not sure if they even will.
But since their emulators were used natively in CCS v6.1, I'm hoping I can get any needed files from TI or another 3rd party.
An expedited answer would be greatly appreciated as I've been working on this for over a week now without any good results, except to know that my emulator seems to be working.