This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Dear Texas Instruments Support,
I am currently working with the TMS320F28P65X microcontroller and testing the flash serial programming example using serial_flash_programmer.exe. The process is functional; however, I am experiencing extremely slow transfer speeds while loading the flash kernel into RAM via SCI boot mode.
To troubleshoot the issue, I modified my setup by connecting the XDS110 application/user COM UART to SCIA through the XDS110 Target Interface connector and GPIO12 and GPIO13.
Command used: serial_flash_programmer.exe -d f28p65x -a led_ex1_c28x_dual_blinky_cpu1.txt -n led_ex1_c28x_dual_blinky_cpu2.txt -b 34800 -p COM4 -v
My final goal is to download the flash kernel to Flash, so that the microcontroller can always boot from Flash instead of requiring loading the kernel. Once I have the kernel in Flash, I plan to modify both the flash kernel and the flash serial application to use the custom protocol already implemented in my powertrain system for compatibility.
Any guidance on reducing the kernel load time, optimizing the bootloader process, and implementing a Flash-based boot approach would be greatly appreciated.
Best regards,
Luciano Vittori
Sorry: the used command was:
./serial_flash_programmer.exe -d f28p65x -k flash_kernel_c28x_dual_ex1_c28x1.txt -a led_ex1_c28x_dual_blinky_cpu1.txt -n led_ex1_c28x_dual_blinky_cpu2.txt -b 34800 -p COM7 -v
Hi Luciano,
The 16ms inter-byte delay comes from the overhead required to read the data from COM ports on Windows. The serial flash programmer is reading the echoed back data from the target one byte at a time so this 16ms delay creates quite a loss in performance. You could try ending other tasks running on your PC except for the ones necessary for loading the kernel to the device as there may be some tasks with higher priority than the exe. Additionally, you could modify the host/kernel code to not rely on byte-by-byte verification (checksum).
To create a flash kernel that resides in flash, you'll have to start by modifying the linker cmd file to place the appropriate sections in flash. You can refer to 28p65x_flash_api_lnk_CPU1.cmd in C2000Ware_Install_Location\C2000Ware_5_04_00_00\device_support\f28p65x\common\cmd. You can place the kernel in any of the banks available to CPU1 based on your desired behavior.
Some other questions to consider when converting the existing flash kernel to a flash-based application:
If you give me some more details on your desired behavior, I can provide more guidance.
Kind regards,
Skyler
Hello Skyler,
Thank you for your response.
So, you are suggesting that the delay is caused by the operating system rather than the host application and that I could mitigate this issue by bypassing verification and sending bytes without reading the port.
In my current system, the flash kernel always executes at startup with a timeout, so I want to maintain this approach. Since I am new to the Texas Instruments environment and bootloader development, I plan to make progressive changes.
I believe I need to program the flash kernel in a separate bank from the application. My idea is:
My next step is to program the flash using the same host application, making modifications only to the flash kernel and application command files.
Does that make sense?
Hi Luciano,
I wouldn't recommend fully bypassing a verification method, but if the byte-by-byte verification is too slow then an alternate approach could be considered. Without any sort of verification, you risk writing a bunch of garbage to your device.
I plan to modify both the flash kernel and the flash serial application to use the custom protocol already implemented in my powertrain system for compatibility.
Does your protocol mentioned here rely on the SCI communication with your host PC?
It's not a requirement to have the kernel be separate from the application, but it does make your implementation a lot easier. The next steps you described make sense, please reach out if you have any more questions!
Kind regards,
Skyler
Hello Skyler,
My protocol relies on CAN communication, but I believe that if I can make this example work as a resident bootloader, modifying the application logic later will be easier for me. My plan is to make progressive modifications to fully understand the process and ensure that everything works correctly.
I have modified the command files for the Flash Kernel and the CPU1 and CPU2 applications, but unfortunately, it is still not working.
I can successfully communicate with the host and execute commands such as DFU1, DFU2, Verify CPU1, and Verify CPU2. However, when I try to Run CPU1, the LEDs do not blink. I verified that the application is correctly programmed in Flash at 0x0A0000 (CPU1) and 0x0E0000 (CPU2), but the application does not seem to be running.
I don't know How to upload files here so I've uploaded projects on GitLab to share with you
28p65x_flash_programming_cpu1tocpu2_FLASH_28p65
28p65x_generic_flash_lnk_cpu1
28p65x_generic_flash_lnk_cpu2
Do you have any ideas on what could be causing this issue?
Thank you in advance!
Hi Luciano,
My protocol relies on CAN communication, but I believe that if I can make this example work as a resident bootloader, modifying the application logic later will be easier for me. My plan is to make progressive modifications to fully understand the process and ensure that everything works correctly.
When you decide to port your implementation over to CAN, we also have similar examples for both classical-CAN and CAN-FD on this device. There are some differences in the user experience between the SCI and CAN examples, but the underlying implementation is very similar.
What behavior do you see when you send the RUN CPU1 command? Does the device branch to the expected entry address at 0xA0000? I recommend stepping through your bootloader to see if it branches to the proper address or if it hits an NMI/unexpected behavior after branching. If the bootloader branches to the correct address and then the LEDs aren't blinking, then it's likely an issue with the LED project. Does the LED project work when you load it via CCS?
Kind regards,
Skyler
Hello Skyler,
Thank you for your response.
When you decide to port your implementation over to CAN, we also have similar examples for both classical-CAN and CAN-FD on this device. There are some differences in the user experience between the SCI and CAN examples, but the underlying implementation is very similar.
Yes, I plan to explore those examples later as I progress in my implementation. Right now, my priority is to make this example work as a resident bootloader so that I can fully understand the process before transitioning to CAN.
What behavior do you see when you send the RUN CPU1 command? Does the device branch to the expected entry address at 0xA0000? I recommend stepping through your bootloader to see if it branches to the proper address or if it hits an NMI/unexpected behavior after branching. If the bootloader branches to the correct address and then the LEDs aren't blinking, then it's likely an issue with the LED project. Does the LED project work when you load it via CCS?
I started a debug session and placed a breakpoint at the end of the Flash Kernel execution. At that point, the entry address is correctly set to 0x0A0000.
return(EntryAddr);
I continued stepping through the execution and observed that at the end of the assembler file (f28p65x_codestartbranch_cpu1.asm
), after the LRETR
instruction, the PC (Program Counter) is set to 0x0A0000
.
However, since this is a Flash Kernel debug session, I lose visibility of what the code is executing after this jump.
I know the LED blinky application is working, because before modifying the command files, I tested it. But I have just found a key point here:
I tested the original example again, loading the Flash Kernel into RAM, both via CCS or by the SCI loader and then tried Run CPU1, but the behavior was the same. In that case, the LED blinky application executed correctly, but only after a hardware reset.
I suspect that I am not handling the transition correctly or that I am misusing the host application.
How should I proceed to ensure a proper transition and execution?
I hope this helps clarify my current status. Let me know if you need any additional details.
Hi Luciano,
However, since this is a Flash Kernel debug session, I lose visibility of what the code is executing after this jump.
You can load the symbols associated with the LED blinky example to see what is happening when you branch to 0xA0000. Load -> Load Symbols -> select the .out file associated with your CPU1 LED blinky application.
Kind regards,
Skyler
Hi Skyler,
You can load the symbols associated with the LED blinky example to see what is happening when you branch to 0xA0000. Load -> Load Symbols -> select the .out file associated with your CPU1 LED blinky application.
That sounds really interesting! I’m not very experienced with debugging, so I’m not entirely sure how to do that step correctly.
That being said, I believe I was using outdated files. After recompiling and testing everything again, I can confirm that the Flash Kernel as a resident bootloader is now working! So, the last project I mentioned is now fully functional.
Thank you very much for your support!
Best Regards,
Luciano